SIW 6AT-A22 with adaptive torque

PUT AWAY YOUR TORQUE WRENCH

Achieve ETA certification for anchor bolt installation into concrete with the introduction of the new Adaptive Torque System

Over-torqued and under-torqued anchors are among the most common causes of failed jobsite inspections.

Independent studies have identified poor construction procedures as one of the main causes of structural failure, while the American Construction Inspector Association reveal that over-and under-torqued anchors are the number-two reason for failed jobsite inspections.

And maybe it is no wonder, when the available tools do not match the current demands. To correctly install an anchor your choices are between a slow and imprecise torque wrench, cumbersome torque bars or a powered impact wrench, which lets productivity soar while safety and reliability slump.

Now, with Hilti's Adaptive Torque (AT) system, you don’t have to compromise.


The AT system is made up of three components:

  • SIW 6AT-A22 cordless impact wrench: it looks and works like the previous Hilti SIW 22-A cordless impact wrench but is equipped with intelligent electronics, a more robust anvil and a sleeker nose which can reach into tighter spaces.
  • SI-AT-A22 AT module: a small, very light interface which slots in between the impact wrench and battery. It crunches live data from the SIW 6AT-A22 to recognise when an anchor has been correctly installed.
  • Documentation software: Ensures that the AT module's job history can be transferred to a computer and used to create a detailed installation certificate.

AT-ready tools are equipped with the sensors and on-board intelligence to confirm if an anchor has been torqued according to ETA approvals. The operator simply inputs which anchor is being used – simply by scanning the box with the AT module integrated barcode reader – and the tool does the rest. Afterwards, the tool can be connected to a computer to instantly generate an installation report, offering inspectors and specifiers a guarantee that the work has been carried out exactly as specified.

Simple, Fast, Effective

Select your anchor

Use the AT module’s built-in scanner to read the barcode on your box of anchors. The SIW 6AT-A22 impact wrench then adjusts the torque setting to meet certification requirements. Tap the lock button to confirm your selection and proceed with your application.

Pull the trigger

With the SIW 6AT-A22 impact wrench, all you need to do is pull the trigger and let the tool work. As soon as the SI-AT module lights up green, you know the anchor has been torqued to exactly the right level to comply with ETA approvals.

Adjust and retorque

Sensors in the SIW 6AT-A22 recognise if an anchor has been loosened and, on retightening, will restore the correct torque, giving you confidence that the anchor has been correctly installed. With the AT System you can adjust and re-torque up to three times.

Easily generate your installation report

Simply connect the AT module to a computer using a standard USB cable

Full accountability has never been easier: Simply connect the AT module to a computer using a standard USB cable and the AT Documentation Software then downloads performance data stored by the SI-AT-A22 AT module, which can then be used to produce an installation report.

The report lists all products used, the method of selection (scan or manual) and completion time and date.  

From a specifier’s perspective, this report proves that the anchors have been correctly installed and meet certification requirements. From an installer’s point of view, it can help you breeze through site inspections with confidence.

Change is encouraged

Intelligent impact wrench

The SIW 6AT-A22 impact wrench is intelligent enough to detect an anchor which has been tightened and then loosened again, a function which is useful for straightening or aligning neighbouring fixtures, such as railings and windows.

During this process, the SI-AT-A22 AT module will use an algorithm, developed from over 10,000 tests, to re-tighten the anchor ensuring no over-torqueing occurs. Once complete, SI-AT-A22 provides a visual indication to the operator by flashing a yellow light, displaying a notification and playing a sound.

Safety, productivity, approval

Please enter alternative text here (optional)

SafeSet is the proven methodology from Hilti for consistently high-quality anchor installation at lightning speed.

The SIW 6AT-A22, along with the AT module, fulfils all SafeSet criteria because they save time and reduce costs while also removing scope for installation error.

Profis Anchor

Discover how Profis software can help you

The PROFIS software suite helps you design anchor fastenings for seismic applications, fatigue loading or dynamic loading.

Learn More
What's New

What's New

Check-out our latest products and services.

Find out more

Share